Gas Mixture

 
Gas mixtures allows you to specify the fill between panes of a multi-pane glazing construction with a mixture of two, three or four different gases. Air, argon, krypton and xenon are available as options. The required properties are: thickness of the gap and the percentages of each of the gas types that make up the mixture. Note that the sum of the percentages should equal 100.