Simulation Method

 
Simulation Method controls the Simulation method which determines how the alternatives in the project will be calculated. There are two Simulation Methods
·         Load Design: Will calculate only the Load and Design
·         Energy and Economic: Will calculate Load Design, Energy and Economics
 
The Simulation Method selection can be made in two different screens.
1.       New project screen
The project defaults display the default setting, but will allow changing the Simulation Methodology per project.
2.       Calculate results screen
When the user has an Energy and Economics license, the simulation Methodology might be chosen as Energy and Economics to run every alternative with that methodology or Per Alternative. Load Design licenses will only allow to run it as Load Design.