Utility Peak Demand Summary

 
Utility Peak Demand Summary
The Utility Peak Demand Summary report provides you with a monthly profile of the peak demand for each fuel type utilized on a project. The report breaks the monthly peak demand down to usage type categories including Heating, Cooling, Interior Lighting, Exterior Lighting, Interior Receptacles, Exterior Equipment, Fans, Pumps, Heat Rejection, Humidification, Heat Recovery, Water Systems, Refrigeration, and Generators. This report also provides when the monthly peak occurs. The graph depicts the tabular data, with colors noted in the legend. 
 
In the example below, the peak electric demand of the small building is 18 kW in January and 43.7 kW in July. In July, 28.5 kW of the 43.7 kW was due to cooling equipment. The peak kW does not account for high amp draw upon motor start up; this means the engine intrinsically assumes all devices have soft starts. 
 
Summary of each category: 
Heating: 
 
All heating equipment including consumers associated with their equipment libraries. For example, electric heating coils, electric boilers, boiler parasitic loads. This does not include fans or pumps defined separately in the loop. 
Cooling: 
 
All cooling equipment including consumers associated with their equipment libraries. For example, DX cooling coil and its crankcase heater, air cooled piece of equipment and its condenser fan, water cooled chiller, cooling mode of operation for a heat pump. This does not include fans or pumps defined separately in the loop. 
Interior Lighting: 
 
Interior lighting defined in the internal load properties on the Create Building tab. 
Exterior Lighting: 
 
Exterior lighting defined in the Create Site tab. 
Interior Equipment: 
 
Miscellaneous equipment defined in the internal load properties on the Create Building tab. 
Exterior Equipment: 
 
Exterior Fuel Equipment from the Power-Using Objects toolbar on the Create Site tab. 
Fans: 
 
All fans (supply, return, OA, exhaust) but does not include condenser fans. 
Pumps: 
 
All pumps in loops defined in Create Plants. 
Heat Rejection: 
 
This includes both the condenser fan and the basin heater for condenser loops defined in Create Plants. 
Humidification: 
 
Humidifiers defined in Create Systems. 
Heat Recovery: 
 
Energy consumption associated with airside energy recovery devices. This is not the amount of energy recovered.  This does not include waterside heat recovery. 
Water Systems: 
 
Exterior Water Equipment from the Power-Using Objects toolbar on the Create Site tab. 
Refrigeration: 
 
Not used. 
Generators: 
 
This is the fuel used by Internal Combustion Engine and Combustion Turbine from the Power-Generating Objects toolbar on the Create Site tab. This is the fuel consumed, not the generator power. 
Electricity Produced: 
 
This is the total energy produced by all generators on the Create Site tab. 
 
Details of each category: 
Heating 
  • Plant Water Heater 
  • VRF Indoor Units (Heating Mode) 
  • Water Source Heat Pump (Heating Mode) 
  • Electric Heating Coils 
  • Gas Heating Coils 
  • Air-to-Air Heat Pump (Heating Mode) 
  • VRF Air-Cooled Outdoor Unit (Heating Mode) 
  • VRF Water-Cooled Outdoor Unit (Heating Mode) 
  • Electric Baseboard Heaters 
  • In-Floor Electric Heating 
  • Parasitic Boiler Loads 
Cooling 
  • Absorption Chillers 
  • Combustion Turbine Chillers 
  • Engine Driven Chillers 
  • Electric Chillers 
  • Water-to-Water Heat Pumps 
  • VRF Indoor Units (Cooling Mode) 
  • Water-Cooled DX Components 
  • Water Source Heat Pump (Cooling Mode) 
  • Air-Cooled Unitary DX Components 
  • Air-to-Air Heat Pump (Cooling Mode) 
  • Split Faced Air-Cooled DX Components 
  • VRF Air-Cooled Outdoor Unit (Cooling Mode) 
  • VRF Water-Cooled Outdoor Unit (Cooling Mode) 
  • Dehumidifier 
  • Evaporative cooler 
  • Energy recovery ventilator 
  • Direct evaporative cooling 
  • Indirect evaporative cooling 
  • Zone Equipment Fans (if included in energy rate of equipment) 
Interior Lights 
  • All room light loads designated for energy consumption. 
Exterior Lights 
  • Exterior Lights on the Create Site tab. 
Interior Equipment 
  • All room miscellaneous loads designated for energy consumption. 
Exterior Equipment 
  • Exterior Fuel Equipment on the Create Site tab. 
Fans 
  • Does not include heat rejection fans, such as condenser fans or cooling tower fans. 
  • System Main Fans 
  • System Return Fans 
  • System Exhaust Fans 
  • Room Exhaust Fans 
  • Zone Terminal Box Fans 
Pumps 
  • All pumps on any plant loop. 
Heat Rejection 
  • Cooling Towers 
  • Dry Fluid Coolers 
  • Evaporative Fluid Coolers 
Humidification 
  • Electric Steam Humidifier 
  • Gas Steam Humidifier 
Heat Recovery 
  • Desiccant Air Heat Exchangers 
  • Flat Plate Air Heat Exchangers 
  • Sensible and Latent Air Heat Exchangers 
Water Systems 
  • Standalone Water Heater in the room properties. 
  • Exterior Water Equipment on the Create Site tab. 
Refrigeration 
  • None 
Generators 
  • Combustion Turbine Site Generators on the Create Site tab. 
  • Internal Combustion Engine Site Generators on the Create Site tab. 
Electricity Produced 
  • Photovoltaic (PV) Panels on the Create Site tab. 
  • Wind Turbines on the Create Site tab.