Building Constructions

Building construction library members are created to define the building construction and zone to be applied to the whole building.  Standard library members cannot be edited.
The building construction library member details screen displays the fields that must be defined when creating custom library members, and are pre-determined for standard library members:
●       Name: Name of the building construction template for the library member
●       Source: Where the library member came from (ex. Trane)
●       Description: Brief description of the library member (ex. Standard library by Trane)
The following construction type names must have a library member selected from the drop down menu to the right of the name:
●       Exterior Walls, Ground Contact Walls, Interior Walls, Roofs, Ground Contact Roofs, Ceilings, Exterior Doors, Interior Doors, Raised Floors, Exposed Slabs, Ground Contact Slabs, Interzone Slab, Exterior Windows, Skylights, Interior Windows.
 
 
See the Reference page for resources used in the help documentation.