Trace 3D Plus
User Guide
 
×
 
 
Templates Library
Templates contain information which can be applied to any project. Selecting a template pre-fills data for the following worksheets:
 
 
 
 
Airflows
Airflows library members are created to define the Cooling and Heating Flow Rates, Ventilation, Infiltration and Room Exhaust to be applied to the space.  Standard library members cannot be edited.
The airflows library member details screen displays the fields that must be defined when creating custom library members and are pre-determined for standard library members:
       Name: Name of the airflows template for the library member
       Source: Where the library member came from (ex. Trane)
       Description: Brief description of the library member (ex. Standard library by Trane)
The following fields must be completed to complete the creation of a new airflows library member:
 
 
General
Cooling and Heating Flow Rates
Default: Auto Sized, the option to manually enter a flow rate can be performed by clicking the checkbox to the left of the Auto Size option
Min & Max: N/A
Typical Range: N/A
Units: ACH, CFM, L/s, m3/s, m3/hr
 
Ventilation
Standard
Select the appropriate ventilation Standard from the drop down menu.
 
Type
Per the standard selected above, select the appropriate ventilation Type from the drop down menu.
 
Schedule
Select the appropriate schedule from the drop down menu.
 
People Based Rate/Air Flow Rate
Value and units auto-populate per the ventilation Type selected above.
       People Based Rate option appears when an ASHRAE 62.1 or Title 24 standard is selected
       Air Flow Rate option appears when a general standard is selected
 
Infiltration
Type
Select the appropriate infiltration Type from the drop down menu.
 
Flow Rate
Value and units auto-populate per the infiltration Type selected.
 
Schedule
Select the appropriate schedule from the drop down menu.
 
Room Exhaust
Type
Select the appropriate room exhaust Type from the drop down menu.
 
Flow Rate
Value and units auto-populate per the room exhaust Type selected.
 
Schedule
Select the appropriate schedule from the drop down menu.
 
See the Reference page for resources used in the help documentation.
 
 
Internal Loads
 
Loads library members are created to define People, Light and Misc. Equipment loads to be applied to the space. Standard library members cannot be edited.
The loads library member details screen displays the fields that must be defined when creating custom library members, and are pre-determined for standard library members:
       Name: Name of the loads template for the library member
       Source: Where the library member came from (ex. Trane)
       Description: Brief description of the library member (ex. Standard library by Trane)
 
Loads library member templates can contain the following three loads:
People
Name
Enter the Name to define the people load
 
Percent Floor Area
Enter the Percent Floor Area
       Typical value: 100%
       Range: 0-100%
 
Type
Enter the appropriate Type from the drop down menu 
       This will auto-populate Density, Activity, Sensible Load, Latent Load and the Sensible Radiant percentage per the pre-defined library member
 
Schedule
Select the appropriate Schedule from the drop down menu
 
Light
Name
Enter the Name to define the light load
 
Percent Floor Area
Enter the Percent Floor Area
       Typical value: 100%
       Range: 0-100%
 
Type
Enter the appropriate Type from the drop down menu 
       This will auto-populate Density, Lighting Configuration, Heat into Return Air, Thermal Radiation and Visible Radiation percentage per the pre-defined library member.
 
Schedule
Select the appropriate Schedule from the drop down menu
 
 
Misc. Equipment
Name
Enter the Name to define the Misc. Equipment.
 
Percent Floor Area
Enter the Percent Floor Area
       Typical value: 100%
       Range: 0-100%
 
Type
Enter the appropriate Type from the drop down menu 
       This will auto-populate Density, Utility Only, Fuel Type, Latent, Radiant and Lost Heat percentage per the pre-defined library member.
 
Schedule
Select the appropriate Schedule from the drop down menu.
 
See the Reference page for resources used in the help documentation.
 
 
Building Constructions
Building construction library members are created to define the building construction and zone to be applied to the whole building.  Standard library members cannot be edited.
The building construction library member details screen displays the fields that must be defined when creating custom library members, and are pre-determined for standard library members:
       Name: Name of the building construction template for the library member
       Source: Where the library member came from (ex. Trane)
       Description: Brief description of the library member (ex. Standard library by Trane)
The following construction type names must have a library member selected from the drop down menu to the right of the name:
       Exterior Walls, Ground Contact Walls, Interior Walls, Roofs, Ground Contact Roofs, Ceilings, Exterior Doors, Interior Doors, Raised Floors, Exposed Slabs, Ground Contact Slabs, Interzone Slab, Exterior Windows, Skylights, Interior Windows.
 
 
See the Reference page for resources used in the help documentation.
 
 
Room Types
Room types library members are created to define room loads based on construction, load and airflow library members to be applied to the space.  Standard library members cannot be edited.
The room types library member details screen displays the fields that must be defined when creating custom library members, and are pre-determined for standard library members:
       Name: Name of the room type template for the library member
       Source: Where the library member came from (ex. Trane)
       Description: Brief description of the library member (ex. Standard library by Trane)
       Construction: Select the appropriate room construction type library member from the drop down menu
       Load: Select the appropriate load type library member from the drop down menu
       Airflow: Select the appropriate airflow type library member from the drop down menu
Note: You can click on the gray box to the left of the Construction, Load or Airflow name to view details of the selected library member.
 
 
See the Reference page for resources used in the help documentation.
 
 
Construction
 
Construction library members are created to define room loads based on construction, load and airflow library members to be applied to the space.  Standard library members cannot be edited.
 
The construction library member details screen displays the fields that must be defined when creating custom library members, and are pre-determined for standard library members:
       Name: Name of the construction template for the library member
       Source: Where the library member came from (ex. Trane)
       Description: Brief description of the library member (ex. Standard library by Trane)
The following construction type names must have a library member selected from the drop down menu to the right of the name:
       Exterior Wall, Ground Contact Walls, Roofs, Ground Contact Roofs, Ceilings, Exterior Doors, Raised Floors, Exposed Slabs, Ground Contact Slabs, Exterior Windows, Skylights
 
See the Reference page for resources used in the help documentation.
 
 
Zone Types
Zone types library members are created to define zone loads based on zone control inputs to be applied to the space. Standard library members cannot be edited.
 
The zone types library member details screen displays the fields that must be defined when creating custom library members, and are pre-determined for standard library members:
       Name: Name of the zone type template for the library member
       Source: Where the library member came from (ex. Trane)
       Description: Brief description of the library member (ex. Standard library by Trane)
For zone control, click the gray box to view and enter the following library members and set points:
 
       Supply Path: Select the appropriate Supply Path library member from the drop down menu
       Return Path: Select the appropriate Return Path library member from the drop down menu
       Cstat Schedule: Select the appropriate Cstat Schedule library member from the drop down menu
       Cooling Dry Bulb: Enter the appropriate Cooling Dry Bulb temperature
       Cooling Drift Point: Enter the appropriate Cooling Drift Point temperature
       Hstat Schedule: Select the appropriate Hstat Schedule library member from the drop down menu
       Heating Dry Bulb: Enter the appropriate Heating Dry Bulb temperature
       Heating Drift Point: Enter the appropriate Heating Drift Point temperature
       Cooling Ez: Select the appropriate Cooling Ez library member from the drop down menu
       Heating Ez: Select the appropriate Heating Ez library member from the drop down menu
       Er: Select the appropriate Er (Energy Recovery) library member from the drop down menu
 
 
See the Reference page for resources used in the help documentation.