Flat Plate

 
The Flat Plate heat exchanger is an HVAC component where two airstreams cross by each other. It is used to precondition Outside Air by transferring sensible heat with the return air. There are three types of arrangements: counter flow, parallel flow or cross flow. There is no need to enter dimensions since the performance is determined by specifying the design inlet and outlet temperatures, the convection ratio and if it is operating with an economizer and economizer operation.