Load Design
|
Trace 3D Plus provides all of the options and modeling capabilities expected in a comprehensive load analysis tool but combined with a whole new level of usability that makes load design easy. There are two types of licenses that can be purchased:
Jump to:
Interface Selection
Interface Selection is found under Settings on the top toolbar. Interface is the top option under Settings. The user can turn on and off Tooltips, select “Perform Library Reconciliation on Project Open” and turn on or off News Update . A color selection guide is also available for the color used when default values are shown in the program.
|