Multi System
Multiple System DOA
The Multiple System DOA will deliver conditioned outside air to multiple systems using just one DOA unit. At this time, this is only valid for zone level system types.
Multi Sys Cool/Heat
A DOA unit conditions ventilation airflow to the user entered cooling and heating supply air dry bulb temperature. The air is delivered at the system level to multiple systems.
Multi Sys Dehum/Cool or Heat
A DOA unit delivers conditioned outdoor air at a user-specified low humidity ratio dehumidifying the supply airflow without reheating it. The air is delivered at the system level to multiple systems.
Multi Sys Dehum and Reheat
A DOA unit delivers conditioned outdoor air at a “neutral” temperature by dehumidifying the outdoor air to a user-specified low humidity ratio and then reheating it to a user-specified dry bulb that is near the room temperature. The air is delivered at the system level to multiple systems.