System Configuration Screen
After the air path pattern has been chosen, the system configuration screen appears. The airpath is populated with dampers and the demand box. The demand box represents one zone on the system. In order to populate the air path with the rest of the required components, the components box at the top of the screen should be selected. When selected, it will expand to show all available fans, coils, etc. that can be added. The user will click on a specific component and green buttons will appear on the air path diagram where that component can be placed. The user can click on an individual green dot to place the component. The same is true for the Airterminal Devices, Zone Level Equipment, and Controls and Sensors.