Utility Rate Schedules

 
 
Utility Rate schedules are schedules used in Time of Use Utility Rates. They define the rate type that should be applied throughout the year. There is only one sub-type: Time of Use.
 
 
Time of Use Schedules
These schedules are displayed in the Utility Rates Library for rates that define their consumption type as Time of Use.
 
Timestep: 1
Y value 1: Peak
Y value 2: Mid Peak
Y value 3: Shoulder
Y value 4: Off Peak
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time