Continuous Controller Schedules

 
 
Continuous Controller are schedules that define how a specific numeric value varies throughout the year. There are four sub-types:
 
Each sub-type will be displayed in its applicable section of the project. For example, schedules created under the Carbon Dioxide sub-type will be displayed as part of the system properties when defining demand control ventilation.
 
 
Carbon Dioxide Schedules
 
These schedules are displayed in the Configure Systems sub-section under the Outdoor Air Control tab. It defines the PPM setpoint for a system with demand control ventilation reset.
 
Timestep: 1
Grid Interval: 100
Y Precision: 0
Y Min: 0
Y Max: 2000
Y Units: PPM
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Internal Shading Slat Angle Schedules
 
These schedules are displayed in the Exterior and Interior Window constructions that have blinds as their internal shading option. It defines how the angle of a blind varies throughout the year.
 
Timestep: 1
Grid Interval: 10
Y Precision: 0
Y Min: 0
Y Max: 180
Y Units: degrees
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Humidity Ratio Schedules
 
These schedules are displayed in the Configure Systems sub-section under the Controls tab of a specific system or loop. It will be displayed for applicable controls that control supply air reset based on humidity levels.
 
Timestep: 1
Grid Interval: 10
Y Precision: 0
Y Min: 0 (IP) / 0 (SI)
Y Max: 200 (IP) / 50 (SI)
Y Units: grains/lbm (IP) / g/kg (SI)
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Humidistat Schedules
 
These schedules are displayed in the Configure Systems sub-section under the Controls tab of a specific system or loop. It will be displayed for applicable controls that control supply air reset based on humidity levels.
 
Timestep: 1
Grid Interval: 10
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time