Continuous Controller Schedules
Continuous Controller are schedules that define how a specific numeric value varies throughout the year. There are four sub-types:
Each sub-type will be displayed in its applicable section of the project. For example, schedules created under the Carbon Dioxide sub-type will be displayed as part of the system properties when defining demand control ventilation.
Carbon Dioxide Schedules
These schedules are displayed in the Configure Systems sub-section under the Outdoor Air Control tab. It defines the PPM setpoint for a system with demand control ventilation reset.
|
Timestep: 1
|
|
Grid Interval: 100
|
|
Y Precision: 0
|
|
Y Min: 0
|
|
Y Max: 2000
|
|
Y Units: PPM
|
|
X Min: 12:00 AM
|
|
X Max: 11:59 PM
|
|
X Units: time
|
Internal Shading Slat Angle Schedules
These schedules are displayed in the Exterior and Interior Window constructions that have blinds as their internal shading option. It defines how the angle of a blind varies throughout the year.
|
Timestep: 1
|
|
Grid Interval: 10
|
|
Y Precision: 0
|
|
Y Min: 0
|
|
Y Max: 180
|
|
Y Units: degrees
|
|
X Min: 12:00 AM
|
|
X Max: 11:59 PM
|
|
X Units: time
|
Humidity Ratio Schedules
These schedules are displayed in the Configure Systems sub-section under the Controls tab of a specific system or loop. It will be displayed for applicable controls that control supply air reset based on humidity levels.
|
Timestep: 1
|
|
Grid Interval: 10
|
|
Y Precision: 0
|
|
Y Min: 0 (IP) / 0 (SI)
|
|
Y Max: 200 (IP) / 50 (SI)
|
|
Y Units: grains/lbm (IP) / g/kg (SI)
|
|
X Min: 12:00 AM
|
|
X Max: 11:59 PM
|
|
X Units: time
|
Humidistat Schedules
These schedules are displayed in the Configure Systems sub-section under the Controls tab of a specific system or loop. It will be displayed for applicable controls that control supply air reset based on humidity levels.
|
Timestep: 1
|
|
Grid Interval: 10
|
|
Y Precision: 0
|
|
Y Min: 0
|
|
Y Max: 100
|
|
Y Units: %
|
|
X Min: 12:00 AM
|
|
X Max: 11:59 PM
|
|
X Units: time
|