Project Summary
The Project Summary section displays a Summary of all the alternatives created in the project which reflects if the sections are ready to be calculated. Calculate Results shows the Calculation status, LEED Parameters and allows to Select Time-Series Variables. Standard Reports can be reviewed, printed or Exported from the Reports section. Visualizer is a tool that allows to customize some reports with specific parameters per hour and Simulation Settings allow to change General Settings, Load Design Parameters and Energy Simulation Parameters. 
 
 

Plant and Load only calculation.

It is possible by clicking the below checkbox to calculate load for a plant and demand load only alternative. This requires an alternative to be made without a populated "building and site" tab and "Systems" tab.