Trace 3D Plus
User Guide
 
×

Site Temperature Profile

 
Site Temperature Profile
This report shows the temperature bins of each zone for the 8,760 hours analyzed. The total unmet heating hours are on the left and the total unmet cooling hours are on the right. The zones are organized by system and zone group. See Configure Zone Equipment. This arrangement allows the user to pinpoint the systems and zone equipment that are contributing unmet hours. 
 
In the example below, Zone 203 has 32 unmet heating hours and 14 unmet cooling hours. Zone 203 varies between a minimum of 62.6°F and a maximum of 83.8°F throughout the year, with a mean dry bulb of 70.8°F. Room 203 is between 65°F and 70°F for 3,379 of the 8,760 hours in the year. 
 
Additional information for unmet hours can be found on the Setpoint Not Met Summary.