Temperature Schedules

 
Temperature schedules define how a temperature variable changes throughout the year. There is only one sub-type: Temperature Setpoints. Each sub-type will be displayed in its applicable section of the project. For example, some schedules created under the Temperature Setpoints sub-type will be displayed in the controls section of a loop that has a temperature shut-off control for a piece of equipment.
 
 
Temperature Setpoints Schedules
 
These schedules are displayed in the Building Create Zones under the Zone properties, in the Configure Systems, Configure Plants sub-sections under the Controls tab of a specific system or loop and also in the Equipment Library for equipment that can have variable temperature setpoints.
 
Grid Interval: 10
Y Precision: 0
Y Min: -10
Y Max: 200
Y Units: °F or °C
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time