Temperature Schedules
Temperature schedules define how a temperature variable changes throughout the year. There is only one sub-type: Temperature Setpoints. Each sub-type will be displayed in its applicable section of the project. For example, some schedules created under the Temperature Setpoints sub-type will be displayed in the controls section of a loop that has a temperature shut-off control for a piece of equipment.
Temperature Setpoints Schedules
These schedules are displayed in the Building Create Zones under the Zone properties, in the Configure Systems, Configure Plants sub-sections under the Controls tab of a specific system or loop and also in the Equipment Library for equipment that can have variable temperature setpoints.
|
Grid Interval: 10
|
|
Y Precision: 0
|
|
Y Min: -10
|
|
Y Max: 200
|
|
Y Units: °F or °C
|
|
X Min: 12:00 AM
|
|
X Max: 11:59 PM
|
|
X Units: time
|