Gas Steam Humidifier
This equipment represents a gas fired, self-contained, steam humidifier. It uses gas fired energy to convert ordinary tap water to steam which it then blows or injects into the supply air stream. A blower fan may not be required depending on how the dry steam is delivered into the supply air stream.
The humidifier is controlled to meet the humidity ratio set point of the supply air defined by the associated system humidity controller. If the Rated Power input field is not set to Auto Size, the Full Load Efficiency input specified will be ignored and overridden by a thermal efficiency value determined from the user specified Rated Power, Rated Water Flow Rate, and design conditions for the sizing calculation.
Note: Standard TRACE library members cannot be modified or deleted.

Rated Water Flow Rate
|
Default: Auto Size
|
|
Typical Range: 0.1 to 19 gpm
|
|
Min/Max: 0 to 1,000,000,000,000,000 (this field cannot be left blank)
|
|
Units: gpm; m3/hr; L/s; m3/s
|
This numeric input is the volumetric water flow rate through the humidifier at rated conditions (water entering the dehumidifier at 5.05°C [41.1°F] in m3/s [gpm]).
Rated Power
|
Default: Auto Size
|
|
Typical Range: 25 to 800 kW
|
|
Min/Max: 0 to 1,000,000,000,000,000 (this field cannot be left blank)
|
|
Units: W; kW; Btuh; MBh
|
This field describes the power consumption of the unit, but does not include the electrical consumption of the fan or any standby electrical loads. When the Auto Size option is selected for this field, the rated power value is calculated based upon the value input for the Rated Water Flow Rate, the enthalpy rise of the supplied water from a reference temperature of liquid water at 20°C [68°F] to a saturated steam at 100°C [212°F], and the user defined Full Load Efficiency value.
Full Load Efficiency
|
Default: 90%
|
|
Typical Range: 70 to 95%
|
|
Min/Max: 0 to 1,000,000,000,000,000 (this field cannot be left blank)
|
|
Units: %
|
This input represents the thermal efficiency associated with this object. Note that if the Rated Power input is not selected to be Auto Sized this input will be ignored.
Misc. Power
|
Default: 0 W
|
|
Typical Range: Need to source data
|
|
Min/Max: 0 to 1,000,000,000,000,000 (this field cannot be left blank)
|
|
Units: W; kW; HP
|
This input represents the electrical energy draw associated with this object whenever the schedule for the system it is assigned to indicates that it is available to operate (i.e. regardless of whether or not the humidifier is operating). It is used to capture the electrical energy draw for the controls only.
Fan Rated Power
|
Default: 0 hp
|
|
Typical Range: 0.0001 to 0.0004 kW/(cfm)
|
|
Min/Max: 0 to 1,000,000,000,000,000 (this field cannot be left blank)
|
|
Units: W; kW; hp
|
This field represents the nominal full capacity electric power input to the blower fan for the humidifier. If no blower fan is required to inject the dry steam into the supply air stream, then this input field should be set to zero.