Trace 3D Plus
User Guide
 
×

Discrete Controller Schedules

 
 
Discrete Controller are schedules that have specific options to define how a control or mode of operation changes throughout the year. There is only one sub-type: Internal Shading Control. Each sub-type will be displayed in its applicable section of the project. For example, schedules created under the Internal Shading Control sub-type will be displayed in windows and glass doors what have blinds or shades.
 
 
Internal Shading Control Schedules
 
These schedules are displayed in the Exterior and Interior Window and Glass Door constructions that have blinds or shades as an internal shading option. It defines if the shading is active or inactive.
 
Timestep: 1
Y value 1: On
Y value 2: Off
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time